1) I have created the golden image file with BQ27510-EVM board. Now I need to program it again into evaluation board and to check if all configurations made are proper. The can see that application note "Going to production with the bq275xx" describes the DFI programming for production with firmware coding. Is there any procedure to do the same manually using bqstudio or bqEASY software?
2) I have tried to program the golden image into evaluation board. Though the parameters are updated properly, SOC is not updated. Setting the IT enable bit does not solve the issue. Any further update needed to make it work?