Hello All,
My customer is using our TL431. The Vz is 5.5V, the current is 55mA, the max PCB temp is 75C, please help to calculate what's the TJ temp? is there any risk of this application? thanks
Regards,
Nanfang
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello All,
My customer is using our TL431. The Vz is 5.5V, the current is 55mA, the max PCB temp is 75C, please help to calculate what's the TJ temp? is there any risk of this application? thanks
Regards,
Nanfang
Hello Nanfang,
This device is rated for 100mA, so operating at 55mA should be no problem, but I would recommend that the device junction be held below 125C.
Based on the measurement and calculation you provided, this should be acceptable for the device assuming the junction to case is the best indicator. In order to achieve better thermal performance, I would suggest thick copper traces to each of the pins and the anode to be either connected with a thick copper trace to ground or connected to the ground plane directly to aid in thermal dissipation.
Best,
Michael