This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ78350 Charger Detection

Other Parts Discussed in Thread: BQ78350, BQ78350-R1

HI,

Can BQ78350 detect connection of adapter?

What I want is , smart battery FETs(low side) are disabled during storage,

and if external charger adapter is connected to battery, then FETs should be turned on.

Smart battery also have a MCU on it.

  • The bq78350-R1 does offer the PRES input to detect whether the pack is inserted and turn the FETs on or off depending on the state. If the bq78350-R1 and bq769xx device are in shutdown, then the wake-up detection feature is on the bq769xx device. You can wake the devices up by applying a temporary voltage to TS1.