This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
For all versions of LMS1585A and LMS1587 in the TO-263 / KTT / 3-pin package (1):
RθJA-High K = 40.4˚C/W (2)
RθJC, top = 42.7˚C/W
RθJB = 23.0˚C/W
Psi JT = 9.8˚C/W
Psi JB = 22.0˚C/W
RθJC, bottom = 0.5˚C/W
(1) For more information about traditional and new thermal metrics, see : Semiconductor and IC Package Thermal Metrics application report, SPRA953.
(2) Thermal resistance value RθJA is based on the EIA/JEDEC High-K printed circuit board defined by : JESD51-7 - High Effective Thermal Conductivity Test Board for Leaded Surface Mount Packages.