This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS56C215 -- Max Duty

Other Parts Discussed in Thread: TPS56C215

Team,

 

Our customer is investigating a device which can achieve simultaneously both High Current and High Duty.

 

<< Customer's Spec >>

 Vin = 5.8V - 13.2V

 Vo = 5V

 Io = 8Amax

 

TPS56C215 has Toffmin(max) = 310ns, on the other hand, the device topology is D-Cap3.

I think if D-Cap3 in the device can expand the ON time as long as its boot voltage is kept at low Vin, more than 90% duty can be achieved.

 

Let me confirm whether TPS56C215 can achieve more than 90% duty or not.

 

よろしくお願いします。

Thanks and Regards,

Metropolitan (Tokyo) Area FAE  Kenji Ninagawa