This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63061: Minimum input for 5V /300mA output?

Hi,

Eventhough the input oltage range is from 2.5V to 12V, I've noticed that the minimum input is referenced as 4.2V.

I wanted to know if I can use this product continuously in boost mode for 5V/300mA output with 3.3V input.