My customer designs a power scheme for C6657. They prefer to use PMP7256.
1) There is the L1 = 500nH in a Schematic. Ther is the L1 = 700nH in the BOM. Where is a mistake?
2) This inductance (L1) has a too high profile. Is it possible to change L1 on another inductance with an approximately the same value but a higher DCR (MLC1265-701ML (DCR=1.24mOhm for L=700nH) and IHLP-2525CZ-01 (DCR=5mOhm for L=680nH) ?
Schematic
BOM
L1 from BOM
L1 is low profile