Hello,
I want to use TPS65911 in my design. I am not using any off the shelf processor mentioned in datasheet but something else/customised.
My requirement for voltages ate various DC-DC is-
VDD1 - 1.2V, VDD2 - 1.1V, VIO - 1.5V, LDO1 - 2.5V, LDO2 - 1.2V, LDO3 - 1.1V, LDO4 - Not Used, LDO5 - 1.1V, LDO6 - Not Used, LDO7 - 2.5V, LDO8 - 1.8V
Also I do not have any 5V in my design, hence all the inputs (including VCC7) is 3.3V.
Now, I want to use which part number to use (complete)? and How to program EEPROM for custom settings outputs?
My voltage settings do not match with fixed boot settings.
-Pankaj