Hi all
I have two questions about LM5005.
1.Datasheet P.16 R1,R2,C12
I see the following text.
"when using an external set-point divider it may be necessary to clamp the SD pin at high input voltage conditions."
I don't know high input condition.
How much is this input voltage?
2.Datasheet P.10 Oscillaror and Sync Capability
We use the following equation to calculated Rt value.
Rt=((1/F)-580*10^-9)/135*10^-12
What is the value(135*10^-12)?
I think this value is concerned with Error Amplifier Gain/Phase(Figure 7).
※I understood 580*10^-9 is minimam off time.
Is my understanding correct?
Best Regards,
Sho