I've worked through the component calculations from the LM2577 datasheet, in a spreadsheet, but I'm questioning some of the results, so it occurred to me there may be an official TI calculator for this stuff somewhere. Is there (there should be)? If not, does it make sense that the Iripple(RMS) should be 1.71A for the following inputs:
Vout: 20V
Vf: .5V
Vin(min.): 4.75V
iload(max.): .45A
Not a lot of capacitors meet the Iripple spec (2.6A) based on that iripple(RMS); certainly no SMD parts I can find.
Thanks.