This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ28Z610 Charging Current Variation with Respect to Temperature Range Clarification

Hello,


I was analyzing the visual representation in section 4.2 in the technical reference manual, which shows the different temperature ranges, and I am confused as to the meaning of the various currents for each temperature level. For example, the Low Temp Charging has Current Low, Current Med, and Current High. This is also the same for Standard, Recommended, and High Temperature levels. It makes sense that the current should be adjusted depending on how hot or cold the environment is based on the application, but I don't understand why there exists three different currents for the same temperature rating.

Also, in section 4.2, the TRM states, "The charging algorithm adjusts ChargingCurrent() and ChargingVoltage() according to the temperature range." Now, I know that the gauge is not capable of regulating the current delivered from the charger. It is only capable of turning the FETs on or off. So, my thought was, what was meant by that statement was that the gauge possibly adjusts current protection thresholds as a function of the measured temperature. This seemed contradictory to me since there is already other parameters such as OCC, OCD, OTC, and OTD. Anyways, that was my thought process, and I was wondering if someone could provide insight on the temperature and current levels.

Thank you for your time.

Blake

  • Hi Blake,

    Current Low, Current Med and Current High refer to different voltage levels. Take a look at the table in section 4.4 of the TRM: www.ti.com/.../sluua65b.pdf. ChargingCurrent() is a function of both, temperature and battery voltage.

    The primary use for these current parameters is if you are using a smart charger. They should not impact your protection settings.

    Best Regards,
    Ben Lough