Hi All,
I have a `Solar Study Light Project` for the Africans who has no access to electricity.
Almost 10 different controller board samples that had been designed by several different engineers in China, but all have failed(had a lot of issues).
My technical knowledge about circuit design is very limited, so I am not confident to design by myself at all. So I will appreciate
if someone can help to draw a simple schematics with low cost BOM to let this project light up African children and their families` world.
I have spent a lot of time and I have found 2 ICs that are with lowest cost. Actually I am not sure if these are suitable to implement the below functions,
so if you think there is more suitable and/or more cheaper solutions, it will be much more better.
Solar Chargin IC: BQ24040, Boost Converter: TPS61070
The functions are quite simple;
* Solar Input: 6V-3~5W (if it helps, the solar panel can be set as 9V) by DC1 port. * Battery: 5600mAh Lithium (2x 2600mAh cells)
1- Study Light: 2 modes, 1W - 2W (3.0V/0.33A & 3.2V/0.6A) by 2Pin CONN, and controlled by 3 state Switch1(off/1W/2W)
2- External LED Bulb-1: 2 modes, 0.7A & 1.4A by DC2 port and controlled by 2 state Switch2 (since there is a long cable, I just write the required Ampere)
3- USB Charging: 2 Modes, 5V-1A & 4V-0.9A, controlled by detecting the short or open state of the D- & D+ pins(if open->5V, if short->4V)
All the 3 functions should be able to work simulteanously. If limiting the current with a single resistor does not waste the power,
can ignore the TPS61070 Boost Converter.
If there is another similar priced IC which can handle these items alone, it can be used instead of above ICs.
Really hope to see that this simple controller is not that difficult to fail 10 times.
Thanks,
John