Hi,
I see the spec of Fsw for BUCK3 is typically 1.7MHz, is there a maximum value. Customer got result around 2.2MHz on their board as below. Is it normal or not?
Antony
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I see the spec of Fsw for BUCK3 is typically 1.7MHz, is there a maximum value. Customer got result around 2.2MHz on their board as below. Is it normal or not?
Antony
Hi Antony,
We expect some variation in the switching frequency for BUCK3, BUCK4, and BUCK5 since they are hysteretic converters and the frequency is not well controlled. There are several factors that can effect the switching frequency so I am not concerned that their frequency is a bit higher. We don't expect any issue running at 2.2 MHz.
If they are concerned, they can check the output ripple on their board vs. the EVM. If their inductor is not as high performance, there will be a larger ripple which will cause the hysteretic converter to switch more frequently. It is not unstable, just switching more frequently.