This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MC33063A: Boost SMPS

Genius 5355 points
Other Parts Discussed in Thread: TPS61170, MC33063A

Hi Support,

Input: 5V
Output: 15V
Want to use the circuit to generate 32V @ 100mA max.

Plan to change the R113 to 51K
Vout=1.25(1+R2/R1) = 33.1V

Will there be any issue?
Should I change the inductance value to 170uH?

Thanks.