I have four prototype boards that use the TPS65023. Three of the boards power-up, but one has an issue with nRESPWRON. After the TRESPWRON delay of 128 cycles between 1V and 0.25V (for 100ms), nRESPWRON does not de-assert. I have checked that the 10K pullup is correctly tied to 3.3V. The other three boards do de-assert nRESPWRON after the 128 cycles.
Are there any know issues with nRESPWRON?