This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS75005 PG latches low on input glitch

Other Parts Discussed in Thread: TPS75005

I am using a TPS75005RGWT to power a TMS320F2833 processor (see circuit below).  The voltage monitor is set at 4V.  In general the circuit works fine.

The problem is when there is a brief ( ~10us) glitch on the 5V input sagging slightly below 4 volts, PG goes low and latches in that state.  BTW, the 1.8V and 3.3V are not effected in any way.

I am OK with PG going low during the input glitch, but why does PG latch low, and more importantly how can I configure the TPS75005 so PG returns high after a glitch. Presently input power must be cycled to restore the PG.

Thanks,

Russ