Other Parts Discussed in Thread: TPS54531
Hello,
I'm using the TPS54531 in a design requiring about 4.5A@5VDC (for USB and some other electronics). The problem I'm having is that the TPS54531 literally catches fire or ruptures the housing (and as a result, VIN is always shorted to VOUT afterwards) if I apply 24VDC without pre-charging (slowly ramping) the input voltage.
I have tried both the Webench design, as well as the EVM design. Other things I have tried, to no avail:
-Lower ESR output capacitance (always around 94uF, one electrolytic and two 22uF ceramic)
-SS cap from 0.0082 to 0.01uF
-UVLO on EN pin with resistor divider
-Inductor value of 3.3uH to 6.8uH
-Multiple power supplies
The TPS54531 circuit was completely isolated from the rest of the PCB after the first 2 failures, except 2 0.1uF caps on the output.
Ideas not tested yet:
1. Increase the BOOT capacitor size to 0.22uF
2. Lower ESR input caps
3. Filter cap on the VSENSE input