Hi all,
my customer is using the UCD9090 to generate a power sequencing.
He has downloaded the configuration file from the UCD9090 (base file), then he started a new project from the base file: he has modified it according the needs and has imported the updated file in the base project. In the importing process the changes are seen and the log reports that the changes have been done in the flash.
When the graph with the timing pops, the modified field (delay of first rail) still shows the original value of the base file. The only way to update the device is changing the value in the GUI and applying it to the device (write to Hardware).
Do you see any issue in the process ?
Do you suggest another procedure to program the device from the Fusion GUI ?
thanks,
Domenico