Hello,
I have a question about TPS62065.
SLVS833D describes that the "TEST CONDITIONS" of "R(Discharge)" is "0.8 < VOUT < 3.6 V".
(page-5)
My demand is as follows.
Vin: 4.5V ~ 6V
Vout: approximately 3.8V
Iout: 2A
Special Features: Enable, Output Discharge, Small Package
Can I use the function of the "Output Discharge"?
I worry that 3.8V is beyond the "TEST CONDITIONS".
Regards,
Dice-K