This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LDO (for example, LP2951, ...) in drop out mode?

Hi,

My application needs the LDO with wide input range and low quiescent current, so I intend to use LP2951-33.

Also the LDO has a chance to work in drop out mode (right term?) when the input voltage is below 3.3V (of course I don't expect the LDO can output 3.3V, but I need the output voltage to drive some load at some lower voltage like 2.5V)

Wondering if this possible for LP2951-33? or any other choices as long as wide input range and low quiescent current

Thank you very much