Hi all
I have to make a board(PV Pannel -> Battery charger) PV pannel : 16.5V~21V(Power(w) Max Voltage~open circuit Voltage)
5.75~6.05A(Power Max current~short current)
I'm using TI SM72445 mppt / dc-dc controller
so I purchased an SM72445EVM board
While used under board I have a few problems.
first problem) The input and output are the same.
PV pannel Output Voltage = 18V
SM72445EVM Output Voltage = 18V(No LOAD)
A product that will operate should always be a connection?
Second problem)This may not be a problem.