I will use the LM5141 for a power supply (8-60V -> 5.1V; max. 7A) and try to avoid a current shunt.
According to the datasheet I can use DCR sensing but if the LM should detect an overcurrent at 10A the sensing voltage has to be 75mV. The Rdcr of the inductor is 21mOhm => the voltage on the sensing capacitor is 210mV (at 10A).
1) Can I insert a simple voltage divider on the high side of the sensing line (Vout) or is Vout used internally for additional things?
2) Can I disable the OC detection by connecting CS to Vout?
3) Are there additional parts necessary (I saw an application where they inserted a resistor between Vout and Ccs to compensate the offset).
4) Does DCR sensing affect the loop stability?
I only need an over current protection which will trip between ~10A and ~15A. Can it be done as simple as shown in the datasheet with one resistor and one capacitor?
Thanks for your answers!