We used the TI BQ24295 charger in the product.
1) We met a battery charging issue on the product as follows:
We connected the USB cable to the USB port of NB (Windows 7).
The battery charging became slower later.
1-1) About the details, please refer to the picture below.
2) About the BQ24295
2-1) The Fast Charge Current Limit is set to 1536 mA.
2-2) The Charge Voltage Limit is set to 4.208 V.
2-3) The Thermal Regulation Threshold is set to 120 0C.
2-4) The BQ24295 always displayed Fast & Charging.
3) After the voltage is more than 3.39V, the REG08 of BQ24295:
Bit[7:6] : USB host
Bit[3] : 1
Bit[1] :Normal
Bit[0] : 1
-----------------------------------------------------------------------------------------------------
Could you tell us your comment?
In order to help us debug this issue.
Thank you.