Hi all,
What are min, max value of fpwm at 40Khz?
On datasheet of UCC28070, when 100khz min is 95 and max 105khz. when 290kHz, min is 270 and max is 330.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
The switching frequency tolerance of the UCC28070 is not characterized at 40kHz. However the UCC28070A is functionally equivalent to the UCC28070 and it has a lower minimum switching frequency ( 10kHz as compared to 30kHz). The UCC28070A has a tolerance of + or - 5% from 10.25kHz to 100kHz.
So you should expect a tolerance of 38kHz to 42kHz with the UCC28070.
Regards,
John Griffin