This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR62014 fake chips??

Other Parts Discussed in Thread: LMR62014

We use LMR62014 in a design to convert input voltages of 3.3 to 5V to an output voltage of 6.5V @ 120mA max.

with very good results. Switcher is stable over all line, load and temperature conditions. The design is well

produced in quantities of >3000 per year.

Since approx. one month we encoutered problems with the switcher behaviour in the following manner:

switching frequency rises from 1.6MHz to 2.3MHz

heavy undershoot (1.2V) when internal mosfets switches

approx. 1.2times more input power dissipation

lot of more EMI

We could fix up the problem. Obviously there are two kinds of chip production lots which differ from each other,

GOOD: chip marking top = SH1B, chip marking bottom = 48K, SOT23 thickness = 1.03mm, rounded case

BAD: chip marking top = SH1B, chip marking bottom = 3192, SOT23 thickness = 0.85mm, sharp edged case

Has anyone similar experience with LMR62014?

@TI-engineers: can you confirm chip markings?