Dear TI & Supporting engineers.
I have a quick question.
We have designed a 4P4S battery pack with your BQ40Z60 inside as a "pack side solution" pretty much 100% "copy'n'paste" from the EVM except for the push button and IRQ signals which are not connected
I do have the following signals out of the pack connector:
VSYS, VAC, SDA, SCL, GND
In my application I need to have power from the battery available at all times (as long as there's charge on it at least) and then my system MCU will control power management in my application and talk to the BQ40Z60 etc..
Now I'm a bit concerned as I've been reading your forum and it seems to be suggested that it's not possible to have VSYS available at all times from power on reset?
What I mean is...
Image I have a fresh battery pack (with BQ40Z60 programmed inside) if I then insert that into my product/application I want it to immediately feed voltage on VSYS so that my MCU can boot and monitor the on/off button on my product and take further action if needed
Is this possible?
Have I overlooked something??