Hello;
I am thinking of using TPS54260 for one of my inverting switcher application. Following are the requirements:
1> Vin:24V
2>VOUT=-24V.
3> I.Load:800mA
Load current varies from No load (0mA) to 800mA with a transient peak of 5A.
So my query is does the switcher has any issues at no load condition and also is there any issues with switcher for high peak current for short duration?
Waiting for reply.Thanks