Other Parts Discussed in Thread: TPS65023, TPS65262, TPS65070, TPS65287, TPS65218
Hi team,
I have a requirement below:
1. input 5v, output 1.1V(2A),1.5V(1A),3.3V(0.3A) 1.1V(200mA),1.8V(100mA)
2.we also wants to use I/O as the the controller, when press the pin the PMIC start after 1s, when press again(or press long time), the PMIC stop work.
Thank you.
BR
Frank