Can not get more than 40A output current from UCC27714EVM-551 (rated Vout 12VDC, Iout 50ADC).
With load gradually increasing output voltage drops down 30 mV, output current does not increase above 40A. Further load increase activates hick up mode.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can not get more than 40A output current from UCC27714EVM-551 (rated Vout 12VDC, Iout 50ADC).
With load gradually increasing output voltage drops down 30 mV, output current does not increase above 40A. Further load increase activates hick up mode.
Hello Emil
The EVMs are tested at full load (resistive) before shipping -
I tried my own EVM here in the lab and with Rcs = 220 Ohms the current limit came in at 16A and the peak voltage at the CS pin of the UCC28950 was 2V - as expected.
With Rcs = 110 Ohms the current limit went to 32A.
With Rcs = 48 Ohms the current limit should be above 70A - but I don't have equipment at hand to allow me to load the EVM at 70A - which is why I've been using it with a higher value CS resistor.
I'd double check a couple of simple things - has the CS resistor been damaged - is it still 48 Ohms.
Are you sure that your load is not power limiting ?
It depends of course on what you want to achieve from the EVM, but the Rcs is just a scaling factor and has no affect on the UCC28950 behaviour. One subtlety to be careful of though is that if you use a large value of Rcs the current limit point will come down. The output inductor ripple current will increase in proportion as you reduce the current limit point. For example, let's say you have 10A of ripple, that's 20% at Iout = 50A but 40% at Iout = 25A.
Anyhow. please let me know how you get on.
Regards
Colin