Hi Thomas,
I have a problem, I have this message : "Value is beyond maximum value defined parameter" for the parameter "Design Energy".
I have already had this problem for another parameter.
Can provide myself to me the way of making, or the tool allowing to modify the limits of a parameter?
So, you will find the .bqz as attachment
PK3 c x�:F �) � bcfg/all_data.bcfgx� AE e����>�εN�����r5�\��qv�(F?���j}���3�С4&�5��: ?�v�8�M:�<�>���R��n��yj�63d������#���4-���)�~;��/̤��Oa!�c8 ֠a�'��k��df���c<���� >Ck�����!��&�? ��u�e�k�ĝt���3'7�f���q�P�Z�rʵ��B}�ę����6 Se[i K���ThI(J���G]��]�F�wK��PF�䔤b� �Ph0x3�� kǴ'���Yq��k˥�ZqTh�hӁ��c�<�鴝�Jaą$�W&#��<zE����r4 �-3Fh����e�hb�Xl�e�p����(��'�I�4h�H�H��ɼT�kd��D ����ȷ�S�[�e�U�qb�=iTx��"kV�I�O_��|��|��|�: ꮕ=��o��?�|ׂj�\P�2���F��~��B�=(�=@I2�nc�4�L�>������hFL�i$�(� ��-��m���ޜ�@��"~Y:���E�X�w�Ns�mJ��WEN�s�6R���9Nx��ַ�^�5t��$(_�,��YN*��e� k�`�G�~��f���t9~�(�Q�>1�T-���'q����� ��^ ����ӊ�w�U ��|�J!9u���D_�����5:��ɭ��Z�-r#UC=W4�4�,�K�ߘ�|�z����!��VBie�Hۻ�z;AD�\b�@�U�3�*��([��bHeF�:�%O���S�Y@ ���ɕ���#ni�DP=$<ۄ]1��4��(w���% �0�_���%rN��=���3^�E��M넔����r�i����?I��B(�����@Q� ���ȑ�ƶp�k>N��xW��֛m��i�,,!\����J��͂[9z�ȑ/���?��8.>�������ηá��rVx[/v?�h�D��� +�\B|��ӑ7(�ǜ��fxN�g�ko�A�WM9�����2Rd���_W��&Ԧ?2 B>[?�O�(?�,�l:�6�s�t���cR:V�Yg<�������a�M�{���� �C+��Z����W�YU�*P����I�kD�0($����+�>�Q�B)N�q�[K��/��|�`0Y�9u� �P�p�[��ꨫ \��W ���?f%���T !M��o�=�o�WvW��lPUJ�n�X�V\�ȳ����(�8^ �S/o�ƈ�Mנ{u���5�j��� =nnদKN"�:U���Ie�En{�J�W��/�G�)��p)ٽ!R]"dTY�]���ςQA!s2XK�CT����� �^��#��x-�g���i����戩-D=�fvÙ�}�'^���� H�����"=��e"��!nj-�U�<9�{P��،3�J�i�$rcO�Z���8?W��~�+.���~.�[���%�o8��"�$Ӈ���4l�z �3tYX����{�;s�:���C�BK*��V�o��s4�m�t���Y��1[f�mR�`wK�k��{�|C�b������?�to��l�Aiv��&��ų�e��YZx��M�����J6FW�S@�$��3l�����2�O��Z�+XYbP3vj Np��=�� BR�,h_]�.M���&F��D0���w�R��/��~^�G#��>1�t��k�ĝ�Yg]�֔wlK��{�vLg�(m���GH�`�����;�0Xan�ͫ�h9B�G£�%(ؤ;aa��RQc�(�ph������O���C��呴���!������(�+���c�ƨ�Ι8�1�_�v �ב�6���X��V��y�/i_R��6��'���m��B��>%��ٹ�`�9��2��}�<%��*I�D�n�;�@�X� ��Ϟ�OC���71�f��F�H�Vl�RNN| ��O��켩E��:?�#��F�TG��fT�]X�S��j�� �G�-���k^�K��rR���uE+$�*X�n������k�o�N��t�صX��CU�himfj-01�|�� H��I����n���|�y�]��)40���O���x-����s^ӝq$V�27?�:x�] wt�hk�>��.�r�۵�`��`i�����q�<�j�l| ��T̈�$¹t0� � �*��3fG�e�\��X= �gp�}���@�^��H�ht� ��1�:%���*C� [�bS��s[�`�ڗf�9�ٸY��Hz�F�W��� ����3]�_(o���X>{��Z�Z,ŮlHZ��{m�nk�_����u��l�6�:���V%�������]c��v,��5dOP��-�s��}�fE��I�T��ŵ���O����W?L�맱Nճ�Ț�Թ�x�f�1�-�Y71wp�����F�X�� W�dŞ�{�)Ѡ?뿩P��E��i��)Ԩ'n:v/�S�t�fz��ۣ��`���SaHl�7���pk���Oyu�,��be�e��xA�����BX7WӶ)O�>���U��^2�ؼ���b�:�,��S�p��e9��;_�Ǩ����������3��k�wQu]�Qt>��s�"�=�*̞�Ja�Q���V(b�o�@MC5��n��=M���^��pR�+*[z� ���__I�[����p�F��nLR� ~�6ɮPt��Hd�%�����)왧���8��<��R���N�L#��7�JUJwrg�!L9��$���" ?O��Z�� Vh��բ�? ^��.�iƃ�)�Q'�Va_<!c*I����P*�R3��bi�{9��I?��@����̼=�:�8 A'sgr�9x}Y�{�T���s����+^r���I�c�n\�h��ցi��T��Rfc���[��a�U��@�'�zn�3�Ӯ��ʡY<@�Tv�J�R| ��e"��XpI="E�ZT��jI� ����E������a55�IX�b���j�gb���,K���U�Ŏ�qT�wD��x�67�-MH����:�6{�B=ؤz�����C��v�ϻ-A�����@�����02���U}�B�5g��=`����Q����+XRߟ�0|�K�yk��ˋ�~�~0gTTtg�*vo�6Y����o8�s��LA������p�EC6����Y���M� �}a�d�9��|�����%�G�6ԉ�i�r����[X?�t�y��6������z���8��i,H<)l3`�\�f���}���Y���cw"M�V��6A�o�D����~�ѽS�Ѱ�Z�[�Hi|{g$�_��`�]�M �g\��lz�Ok0�n���T��$s�wE�s�3p�Ǩ"9�`�<�)9v�����.O�y��73l����Bg�]���҇�M���qP�x�J����K����T���GDױG7�;��Ca�U���+���;{�5*;�΄ ����n��a�����-@oV��Y)���%tޖ��7��5(����2�w�w��k`��j�� Kl@ �캺�ߜ���]z�D�]��g��Y_h�!���0�'-4^�R���I9�7�kw�T@���x�$l]z�υx����O�T�s�!�S���ޑ!�P4�R)@�dA*~�-��}zU6�4���v��5:������k�QTJ�J��9m�C�32�E�ȑ�O9���I����}�l� 8��9)NY��D}*>ޙ��6���Z�O�����F�Fq2Z!]�wP]���jћ;�����q3I�\e@��'À�̄��B��fk�C0�җ�لb����O�(f�{r�߬���l���I&" ��9��[^�h�a�qX���R�9��� ����� ���:m*��F�S����!����x�_��~D�3 �=a[q�b6��_^�"2��"%�D�v�1ѭQO(v�q8�:�����6�����5���bv���T�b��~����F�y>�2ng;�o���i�n�Ԃ�iӱ!� �5�Pp^��bZN2�U��X�}�.fs�[�s.��ӛ�$n �ݶ�I��0�z�In��H*ݙU��7�ߨzA7.ۖ�l0+���<8e�E>ɶ|ճ�;�t uM��4SZ�$9��9���g!$! ��ୖ�n�J��W2xuS��&�P}��<��@�W;W�,���>�WbDm'�����0���>��Q�Smi�!�c߂~h�$�d��VN%J�'�=PS K��M�Җ|y��#�!�oY_�=����rjڧ_���0&q^_$�h��K��p3:F㋆�<vvݻ��-���^>�-��;C�_CYH��H���J�q �A���`|�B�6�p�*��� '��uh|oV6Sa���t*7�1��L)X`/V�qn�)� ���q������T������C:�u�(�������WW�>�h��s��W�� :��FIH��ӏ�e�R���� 5����xe�(~�Z� ��p�t5 /v�= #+6g��ؔ��� �p�v����� %�(�:�� ��W����(ՕqG�i�I��%��s/�* �=+����$ ��nS֒������B������<����ƾ���9�7�[-ɲ�k�xrƬ8��2(�Q�wb�7 �-�{˫����܀��/$`��.�]C;��T��<¤�V�FJ���)�����9����YO �|��tT�I���oS�}����5V2Z$pR��h�r�O��p�#Md�=8��:�>}? B��愘�`߬2���p�� ��#z�R���LO� /.`7���� ���I� t<�8J�[j�B���(�ON���{������QO�\L���j�P��qr�B*Px��2���Vq��&R�����z`���j�����<����`t�!�o ֖q����*�>����9��f�ޏ��ECݬz��4��,�Ë�^=P��YJFd�i"�<��[FW�0����q���'O���u��A+Y�@$$�R73�1�~h����!I�?�ԩh�n8�=�� ZGGs@�*d������d��~K�@��4 ���L�D�c\Iݵ�W�.͜ ��ʃb���j�ѱ�m��o�H7Y)NX(/Ў_O�j���$�Ʀ���%_�.�[8�^�I[�B�����4�H0��ƆMbOܤj��X�h���]j�]�_����I&�ݨ��/�����-�abA���N��j�;��+ү�C k ���#@��l��������;i]��Z����m��(h�!�ɼh'�H���Z_�"�/c��j�;�wdN��<o��W��!J��l�e��R�6���_q`2DPsB��F8�v��Bf2eBp[�c� ����X�]j̇�(�U�y��j ��!��>Zf,I<�����<ڍM��^�uB�.��h[$B�^�%� @ N�/�̤C��і"�Q�JW�0�5F�6ݡ�C�|��0�� ���E�nC�M�i6@�)����=�s�����H��K��W���I�*6,�-v7m-��-|� �]E�O�4GcC�E�;L Rq���$�6f�'�1�m����G�e}��c8|����3�.Q��t��"2�!�/ǎ��� �����fە�%x��|�7W Y��r� ���6���.;�<�� ���@�__��Пެȷ<�� �FnE�cA��=�`:�7��E���p2v*�b���p!��?��T<T�-��rO�G���N�1�tƟ�㩥,����fKȃ����O�Q�[�ۤ�/,�a�w��}�q����?��?u�ZA5�@��/m�&(�_:�&�5G, ��C�~3���댌2��bB�R5��@��@����<�e��g�7Zl-�xyn9�d[P��'C����t�ʹ�0���q;�6� S.:m��$�]H �ݣ�n��W�Q�ȧ/)�nީȂ�O� u�[�j@wewC*nJ��Dq�L��Cː�p��{P�.�I�f�4�� :�Mb�Ô>��(1P�D�\ُ}���@�g�����w��Km�b�Ƃ���.��/�5��~�w�U�(��xw���oL���Nx�� �����5í�E5_VKl��N �E�m�F�m�̮f�DOKn��d�1i��m*J�LΕ�Ps�>Am��v-���Z�~Op4�ҷD�j6x֘&s��Q���|84Wkn�_(9t��3�E 3Pʮd�TH�&{|$�;YܱF���QAs�Dp���++���a�':���~y����R���ï�B�t�'Uy���2�`;�mF6��P�LY0������5nȹ4��q\ާ�j#/��t�EӋ1!��S�<>��f����w������D�§�~�KU�P�̻O� ��;�q(ѫ���a��rZ�<\�������z����x� ���5�r����^ݵ 77��\H�q N�Fy�>��yRU�\���1� i9�ӳ���m��p�]��6�o��/��X�~�\�&ekr�` � Q-�R�����{@R[Ż���*i�$��h�)���8 t�S\���&K/&'WJ$�i��egq ǍR����#ӆ�S�AT8�tz)� 8n��+z���\E�"jJ%G��,��4�{�0x��'��Xr(y�� 妓����#����?�Ԫ�B�Ӏ��ՁfAh!�(���3�t�QJ��D�)> .�f��.7!F$\����I�I܌>}������u:�;r�iD0���0۬��Kk���)�ȘM8�~5}:�^��}�V�8���yl���Ϣ�e���)]��?���ʘrgiQ�+Xi�n�T�{'�A���<��%���7�*���L�m=��H#�3�>��#�=ۢ�o��s�9�0���������������w�"QM�m]��T�T�����q-�+HNJ�ٔ�;�Z�6� ��Jg�SW�C8E��rGz��^�O��6�+'K�]N��Z;�W�l~_��^7�u�c2ٖl��C5aO��� �|��h&y��)�q��t���A��·Vvq�S�^V�*[�P��s�k8��Mj�}{�.w'�����v7@�kc?��s��ا���߈�1'�䢶(Ӆ���'�hָ�U�[�� U��z��V��E;@��RI�������#��yAb��7ݴ��?�͙����J��8�lv�7''�fYl���+���*o�oR�x���"�[�'���D����Wl�m �q�9���3�s&nZ.$ߥs��\X�ɡ��4���ov���>g�19��숩��k�8���� ۢmP�u�Jӆ��XN�Թ_�C?����^곥�Q�E3��Z�[�3%>���b�~��E��.�G��ĽY9��l.-��*\����$R�E��و6���v�������l�~i�bie�b ��;��V�+�IC �L��K�̼���U�eK8���y�������w�?kKBC�a ��v�Wp���V���1R�@�J ڢ���ą�BE��V&R̅��hM�fŽ�1���ȅD-M�+�i0$��ݢ*�O�mL�c��_�����H��m��@)���x ������;��:� �Sk��iZ�r��0��F�{ ���15��p�����Z���ׂ�~����xFX��ƨ�5}�S�U��"����Zm����=�R�-��̏ ��5[�=�m�o�.V�4c�3��Y�b��Yd('�-P��L&����-�iY�N���/�C��7���{�Ӗd�����,�debQyG ��I��"���ON�ulU� �60�º��r~�N]GPq�c:r�f��L9%l�MB�! J��U��}A�c�L�N��CI�.�ke1���7=0b�!�ۊ�h��y��ޟ/v6a�(��,{�n�[jN�a�r�rvQL�"3^�X����lQ��Az�K@���?Q"l�f���00v9y��x�=� ��˷���.+�8�ר ���mI����0�`>!@�㬤�y�u������]�0�����1����M�8^��������y����_�Z�i��S^ڌߏ�zl��)�W�GC���c!��̑k��3c����}���,� 2��e� -7��<3�ѩjV����%��x�( 0ơ���W^��'��osN~�������;��we�b�:�U�c�+�~��CJzX��� �|&�J%�m���V�.���;/I:R���O#�Q�4��L0��ޡFfpn��Qb�5&U�9�����2,j|��\7�kۿY�������Yo�7��_O4V����m.�n��ej���6���X4�;�M��J�`�-��H`�Xk�@ZV� !x�o *RqS`X���a D��A@��&Oh�E*��ߧ���G}[��0��g����a,R�� ��ܨïJ75.-h�^g\����CbO�&T3��#Fh�dž�o^M���tS������V�l��U>�{������P���<:_.�8 �_nt��wrf����g��HS涢̞� ��(o�;�/ּH/Ѧ{+��jųO�j�nˀ��jn Ӗ�yB��軝I�[�H6�d�� �_���i�d�f (���#?B �m���n�]� �P��[�l���p?6��N�[�r����E�sz��nJ٭��%�<A��e�Z�W�pS�1-o�qq$��y>�}O��J�g�Zg��]ʞU��)�@K��~�3X�|9}�r��hG2������:U���P�Gn.J���s������ �6���3�vz�e�#��v�r~n�ٿ� �5}thz]�/�[֛h0��>Ѷ��|��:��x��>>(}�\<� �@�xʵ��� o�4VR���i1����� rql� rYu���Cʛl��R7H��o�`��E"���.fw�A���:p�;�`Z�Rup�o ���Y�V��];��a�-��R��qΜ2~��3��A4?����_�(fg��/�wm���Td8��M�D���L�BE������]���%"�\��Su�f�6rv7IHV@MW�'A����M�������֨�ݺM��7�l?�k+�a�7¹��3�վĸ�x� �٬�X�j�A ��a�mb���R @J=����h�XF����)�b���HԤb��3�k�����5�����L��.���R�~���k)I�]WA�Xa1�?걺��@�7x�N��N�Z R�ŏ�8|WbyTK�����Y����e��5�}|��F�g �>�T�������@yK_�\)����|~uC�ԭ�W��,�p����t� ��PW&�a�t��4�B�iȭ$,�rM��r�/�����S�8�4�m!�>b`5�ksЉ��+�����CUZ�vIÌR�ū��B$^�X�$s��[�� ���y)���NS[��r��>xg�mM�¤0�l�]���?�r6��;Sη�ř��� "�ǯ�V��EIn�,67����"�}��<��#��1��%�4�R�=��ǟ���\�����<)��? \;�+~��ŏ�"~ �yĞ�����������)�B��r+ ��^�hdU�OW� Oo�?A}r�4-J- �6�J�*S4y7�z���Z������q�soC��ޝ��[(��bZv� �ۉ>2�-�I�) @bfѾԡPQ�J� n�J�høY�A�C !�7ߟ�rD{-�S.� ̯k��b�yw7�ϔ�i����B;�b�N��1�Cq���E�����/l^�BK1�b�I��g������(��+��jx�CϿ�M{� #��U�t�>�q�K#F���I'��b$��zXD�d%�Ѵ�Z�2�7p#��KP�x"� ���c�[{<Յ9,džRM�T;�1�_,�/��d�8�,�n(� 3���Rd@B.E�a�DI�����5���ti��}��� A��)ҧc��Hr��S����rA�H^a�'�{�L��%o�d������ ǢV�g�M��d\�v�M�[j��)��/y��BFyI^�U�?���Q~��(d��%�!$�0��9!J6�0� ���k�[u�߬P�z��·T��/��`�8��G!l&�h�)$�K�I�'�5�h\����v�S7���y.�'3�7�6�IO�R����k@Hu�{g��\1��l-[�4���j���0V��l��84LC��ߐ!���=�D��C�&�l3|��DXo��~y��1�d-{B��<��9|Ժ���L l�7��K��Qڲ���g��B>U7I�k��^kLBG��j.�{��i,Ô�~W3�Pթ�� ���J�߂w�j����_���G1>�;��˄���l�9֑����S6(����Mk4����9��/=:'a�|�f`?vET`b ם�DK%<{�Q0�YL���=2g:�*�]��B��$�2���u�M�D+_;�4����\�����]jy�Ç���>���>�);�����c�\ |2vΆ*�O[���M@��o�'��PK ]uE�{��& � bcfg/main.bcfgxm��n�0E� ����NQ[9aQ�+�j+u���%?�ؐ��� ���;gf�M7�5�(����`��q/�k*����\C"s��dO2�M��Ө�6�{����2,�;�� ������o��b>��\(Ǡ+��ؕÀ��}��)������Ҳ�vɕK�]��O_Ԉ{��t�tr��s�5�AZ�A���LጶCgXT������)�K�u�!���5A�K�W}���6�.^:�O�������m5jY�������P�b� g�7q�̘�`���P|��I�PK NjtEȀ��! bcfg/map.bcfgx��]o�0@�[��!�{I�Q�C�:$�&Ȧ�Y7��X�Gd;�}M�k-hf���s��{��i�Y�(M���~/B�̩(g�W��~�m@��� 3�'=}����r=I��p�K�@W8���% r��J6��Ǚ��J��N����'a��n{�AO�2�E���j��*�ដCԌ��H����^&yh�[��ݢK��iWs���ro�sdWq3�Pz�S�^3mT�� ��Q y�����]d�<<(������hJ ����<�"�6��(NE;劆��9pЁ�����}_~�) 3�"�Bc_�BR*j�$���%�5A9��H�v$��x�lO9��&%��v����sY-YsV!C�R[~���f��p�k�)�D�lG}n�vݼ=�D���n�ǖg�����vx����(�C�F)"N*KV���y��~���ɨc�Ŀq)#ؾ��Յ�pz ���5N�wz��\è۰�������k�GC��{R;������a����9a.~���\���ِ�i��؆t��S�����_ PK �^gET+��� � targetinfo.xml��_o�0��'�;x~O�j�D i�#5c�"�-2�M��حm��/ j�!}���s�<�|]��#�9ؙ�ځ6\�!�]�Ѿ���������e�=W�ܻ!�����tu�4���TM�:��T^u���/Uu��?��ڦ�E�� ��{�pP�������j�hJ �9^��z���_� �_z��>!�5H=c -�8�s ���~�|��[+�R%��L&o$f7Q���<�W]%����U^�>[���ϓ{�8�8x�[�EP[g�2��T���f�?I�G[� �a��11؍��8�^SDJf<_=3j��c*�a� ��R:��k�{�� ����#8CO����l=��hT�K����-���_�E|,hle��aԑ��*��~���϶���B/��D DEɈͳ̀]�EU�� �������۩�PK NjtE��D�� .\ sbs/default.sbsx��n�8��J{Q��f��� -��(MBAC������rBK�j�a�l�|�8���J|^��y���>�}�ۖ��g�Η�S�B�|�,��:���+�.�J����<�6n�V��i)�'ܶD����b��ݖ���CNa:+7:�|��З�K=O��^#ݒ�j�� 5cm�D�m� �+��F���_3�MwZ����AR\�G��k� ��r��F)M�o.�>�<�k�S�g�3�,(hh�cJ� Xz�+n۽FrDI��ʃ���oL��r?��g���������Lc�G"K��k���o�/����a�"{gi^D|H�^��CJ�:>ҁd���d瘾4��$�'*�4��^�i�/m�O��nKݠ'�_��Z&���B�E�T�,A�$�R�|d���1�ጥ���<�ŷ舱@4�.�beS��ƽF�)���[і4�>}T�z�h1mi�ީA��w$}�i� �a�/����(�\24W�L��_q�w�p��N��gI��A�3kt�ҍ"���=QR�8k�Ė�ȣh�E���mIGWd��ؑ�rg��x�\�H^���"���JP6�Z�C��]�����N�fEb����D�����|O�;�4�\TF:�U�U�s��jm`:����-��R���2�N����Ma����YV�`���l֜�cή8gy��]����Aƹ����W�a����_:��8V Vb�^vU��K~��'b5���5'�e\��C��-f�ߡ�gbJ���Z���a���m���Fه����Ͱ��RJۧ��h�iC�w�ޖ'�Q'��p�@� Z����tj��G^O�-��q�p�|܀i��S����-��r5�_� �� ����}����EZ��X�&�jD���!r�%����/y���PyV�u�����0�F� ��8�mQ'sn�W�d�P�1���7+2b1�M{WK��\�4+�;�j���*�h�էbƪ.Bj�P�b��� ���,~�T�Y����qSg�GC��L�dB�'P��ӆv7��a���Xյ��:����<�4ݐg��:,���Q@�O����k�gw}Ea�M�U�IU�U&ڕf}Y1t#Rt3 R7=֛���l�DEF�tT6=|��i���lz>�-;nb�*kΎ)�&u�*�p:*���Ǹ�:;v�nZ�瘞T9�Kae�֥�6"�jU���ݨ�m�����k58(���߉e2�I��c9Lξ��`&���0��ep��.}%�Z��;��G��A�����h�P`.X0x��P�eb(oߏ���&k,[!"����JS)��S �T;�7z���W1�j6Rn"yr��T���y��q�l�D�qz�����P�k��qu�B9�Q��� vp�F���UDF�NTm�d�"2�dH��$7����?��>{�""� �Z�!"�'�cx�n�[d.���~*_\#�Xɷ�$�qU���5z�A����#9R�S�;@�V[�6�I�!S]��Q����EV����{|�Q�,s��LQL���Y�,D��X����U����Xb��s�8XX�o$-�!%��FB!����V�I\�)u��Ma <�#ޗ��Xj�9a�i�.VŽ���W�Z-�mPC���}U�3E3�m����*P!+��/�j�E�<�be��Y��Uɳ���Y�������/PK NjtE�Q�� toolcustomization/commands.xmlݘ�n�6���_m@�X�Ӥ@�B��E���n��(�(%j$�&�ޓ���$;���^:H�,J��8���<���ݥ��TLd�=�u��h��e��^��W�=�4�b�EF�{�T�ލ���,i a�2�B|��`�����d��H�"ZHQ���,��Ln��2�k"T�q,�R#�>;<����������P����ž��i��4"�(#gz̦^�vp�C�2�3��d��/�Yz�ng<s��(�=;,ov�%��$���n&�v�播��� � �U�;3b��}��P]H��K�h.�VH/��7�B!���9K}TEz�.�V8@np���^����D��X�v�o]������]�1]��"}�Ӷ�M>��x�ӫ:nG��0�~"�V� ��x^4�9�.�%��>��xΰ��plv��6x����.d�<�(&����z�o�K��0s��rx�Ql�� ��8"�R�~D���d���$�\���ׁ<��~��4e��4�,aTV[�Msx�vu I���_��m��E!�����S{6�� l�:�okH�x��f'BB��)PJ�*���*-�ʌ��V��@QhM�NC�V�E�e�6~�#�y,��o��;N�E`݊����'M��a?j>�(�D-��Hۢi:��<����蛮���d��6)8�9���h�4ȳ2��t��.��[�t!�0t���s�sY�E=+�o��1;�G�jc����j�շ%U��B�� !;���7��绵��E�0�eU�U9���EhE$#sNUk�a#��ď_qs2<�'���pm18�Z��r*;:9�r,S�7/�6���Ş� B|e��j��`�5�8[��ߺ/��g�Z�ul�!��q�Xb��{��.��7�k��\�S�|�� ��ƽ �KpY�iUy8���F��lPd��?�ܾ�k�J�W�5c��{�ј�'�Xv�M(:whR9��m��h��_���oPK NjtE`0�� S toolcustomization/plugins.xml��A 1E�#x� ���;d����6u��SA]d����5�"���4��P���t4a�M���"+�m�|E� �$)9��(��5)��QӍ��x�A�c�����/b�a��}(H��*RćP���g�PK �`;F�ȣ � toolcustomization/testerinfo.xml���o�0�ߗ���}t{3j��:Ch_+��ڥ-����K\�=Ҝ�9���0�bW�ɪ��+]G�+82m��34�G�u%��l��}���t�OO��e�8��mgŁ���X*�E9�o�~��=F Zۉql� j]�j�T�̊��6{4���V �7�1CYG8��C%�(�������?�<SK��+�� �gLZA��;���g��_Tq�{�t�K��ʆ��6�A��>$����Q��t�ه�����+��U��e�z�L�� \�j�ׁA�ڂ��#�%���U�x�ʽ�����%�� ��$E��>q��κ1�J솇Ԋ_�q��=�Æ^1$q��Qz�ʫ�,-�Y����oNWi�^�4�3%��CXP1t��$����4���HZ�Y�K� �}���+��{�ip��i��PK �T0FpR&�� � toolcustomization/ui.xml�UMs� =�3�;�'�ɥ�L�$�tO��3�V6S* ���]@�L�Cz���-�} ~�n��:i�8�3@]�J��8�|}�-�ʿ~�O=��TX���FxA��S�|����gn��|4d��b8��,�{���n!��`@��rn��B4��Fy����\=�GlZ��w�o���9�E��������� ��RX*#x�!Ŝө������})��Glp�����I*� �S�6��~Ю F�%0�RSo&���|����mVВ����1gS*d�nT��hv�ޢ+�l����k�?.����t&5�J�@(e^ac:�p��A�:PS��y\��lQT���l��@I"Q�:rk,=V���'V҇9h*ԁ *+�a%�4��d'w���[�w2H-��ݧ�~o3�%�>��S;���� RE|���8��,�v��$u�-����8��r�R�Ru�\5q�s�;��ዱU����}[r����Ӊ<P��O�5+����?iS�C�X@�+Y�'�w�&���Q�7sO�.;���X�� �q�{>Jέ�m�#5f�����~�b0y�A�}N� mL��"w���V��HԿ���um8�X]G�$���*����ٷ���p'<���`֠�:�;�d��Crb:e�9�B�Ӻ�M�3ܛ�RR��DZ~ݑ ��2B������/�/PK 3 c x�:F �) � �� bcfg/all_data.bcfgx� AE PK ]uE�{��& � ���) bcfg/main.bcfgxPK NjtEȀ��! ��1+ bcfg/map.bcfgxPK �^gET+��� � ��~- targetinfo.xmlPK NjtE��D�� .\ ��b/ sbs/default.sbsxPK NjtE�Q�� ��36 toolcustomization/commands.xmlPK NjtE`0�� S ��7: toolcustomization/plugins.xmlPK �`;F�ȣ � ���: toolcustomization/testerinfo.xmlPK �T0FpR&�� � ���<