Dear Battery Management Team,
I wanted to ask your advice regarding the following implementation idea: in order to control the charging behaviour via FW command, the possibility to use the shutdown command seem attractive to avoid the charger to deliver power to the pack in a first time interval immediately after it is plugged into the system.
The scenario is the following:
the charger is plugged and the uC sends periodically (i.e. 100ms) the STATE_CONTROL [SHDN] to avoid to charge the battery (DSG fet off); if after few seconds the charger is still present, the charging operation can start, the uC doesn't send the shutdown to BQ77PL900 anymore and the normal operation should be resumed;
The questions are :
- if the SHDN is not sent the normal mode is resumed or does it stay flagged?
- is there any way to restore the normal operation maybe exploiting the State control register?
- how reliable is the operation described above? do you see any critical point?
Thanks
BR
Nicola
In general it would be very helpful if you could comment the conditions to enter/exit the shutdown mode in the scenario above and if there is any way to implement what described above.
Thanks a lot
Nicola