I am currently designing a system for inclusion in smaller solar systems for energy impoverished areas. I am using the 34Z100 but having difficulty getting it to work. The prototype system is 12V/20Ah VRLA. Although in production the systems are both 24V and 12V VRLAs. Because of the capacity (20,000mAh x 2.1V) I must scale (by 2, using Tom 2015 memo). The table below has all of the parameters that I did not leave as defaults:
Parameters | ||
Parameter | Value | Units |
Chemistry ID | 803 | |
Pack Configuration Register | 0x29C1 | |
Number of Cells | 6 | |
Design Capacity | 10000 | mAh |
Design Energy | 21000 | mWh |
Design Energy Scale | 2 | |
Qmax Cell 0 | 10000 | mAh |
CC Threshold | 9000 | mAh |
Load Select | 0 | |
Load Mode | 0 | |
Cell Charge Voltage T1-T2 | 2475 | mV |
Cell Charge Voltage T2-T3 | 2400 | mV |
Cell Charge Voltage T3-T4 | 2325 | mV |
Cell Terminate Voltage | 1700 | mV |
Cell V at Term Chg | 2450 | mV |
I have cycled several times per the directions given by Tom for PbAs in this forum. The UpdateStatus is always 4. The last discharge cycle has rested for ~20hrs and OCVTaken has not come true (it always takes hours).
1. Please give me your thoughts on what I am doing wrong.
2.Should the IT parameters be changed for batteries this large to allow OCV to happen earlier?
3. There are several parameters in the Conf/Charge area related to Pb chemistry (e.g., Pb Reduction Rate) but I cannot find explanations for them.
4. In the Pack Config Register in BQStudio bit 2 of the LSbyte is PB_RESTART which conflicts with the datasheet (p34, QPCCLEAR) and SLUA664 (p13, RSVD) which is it?
Now I am considering following Tom's advice in this forum to convert to the BQ34110 but the datasheet (I realize preliminary) has the words: "Rarely Discharged Applications". Obviously in a PV system the batteries frequently cycle. Is this a contraindication to using this part?
Sorry, for the plethora of questions.