I'm trying to analyze the SAFE circuit transistor switch circuit for a chemical fuse as shown in Fig. 10 of TI doc referenced above. In a 2nd level undervoltage condition, there could be 4.0V available at the battery pack used to blow the fuse; the fuse could have as much as 2.6 ohms heater resistance (Sony SFH-0810C) and the rds(on) of the NDS331N could add another 0.25-0.5 ohms across temp. That could yield only 5 watts across the heater of the fuse, and only 1.4 amps (4V/(2.6+0.25)ohms), best case. Okay, maybe the app note was written for a higher voltage UV (3 cells??) and/or a lower res. fuse. This seems like a stretch, but I guess it works.
But with only 5 watts, it might take 10-20 seconds to blow the fuse. Won't this exceed the SOA rating for this transistor?