I set up the TPS61085 to have the following parameters:
Enable pin controlled by microcontroller (either 0 volts or 5volts)
8V output from a 3V source (power supply at the moment)
650Khz FREQ, 13k/3.3nF COMP circuit
My problem is I get 8 Volts when the microcontroller output pin is high, but I get 2.9 Volts when the microcontroller pin is grounded. I have verified the Enable pin is grounded. Any suggestions? I also verified the schematic is similar to the schematic from the Evaluation Kit (TPS61085EVM)