dear Sir
i am looking for a smallest circuit for LED X 1 solutoin . detail as below. inductorless topology can be accept.
input voltage: 12v form car battery
output: 3.2VLED X1 150mA
Function: no dimming, EN,Low Iq,Open LED protect,high efficiency
PCB size:25.2*6.76*1.6mm
i find the TPS61165 from website but i dont know if it is smallest soluiton.
Sincerely
Tiger