We’ve been using the BQ27621-G1A and we're were surprised that to initialize properly takes seconds and even then, its accuracy is questionable (plus you need to have minimal/no load, so the processor can't be booting during this process). Since I’m currently revising the design, would you suggest continuing with this device or changing it to a more traditional current sense/coulomb counter or something else? As this is battery powered, we need to minimize the sleep current, so whatever the solution is, it needs to be low power (especially when the processor is in deep sleep).