I want LP8758-E0 regulator to power an ASIC that will control it over I2C but some of the default voltages are incorrect. I need to have 1.0V and 1.8V to be enabled by default without needing to toggle ENA pins or register bits, with other 2 outputs disabled (till I2C write) or to have them output different other voltages.
Can OTP memory of the LP8758-E0 regulator be customized by TI per user's needs ?