This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EVM Board -bq40z60 -I/O PINS - Emergency shut down , system present



Hello ,

I need both Emergency shut down as well as precharge function.  It looks both of them are on Pin 14 . Then how to implement that ? 

Venkatramani .

  • The Emergency Shutdown is on pin 15 and pre-charge is on pin 14. There is a pin out error in the datasheet and TRM and they are in the process of being corrected. Please refer to the bq40z60EVM User's Guide for the setups to enable the EMSHUT feature. There is currently a firmware bug that prevents the eternal   pre-charge from working. It will be corrected in the next firmware release.