I'm going to build a custom 4S LiPo BMS. Looking at the available devices on TI I found the bq77905, that looks great to my reach what i want.
But I just have 2 questions
- In my project I just need to monitoring the cells under voltage, over voltage, over current and over temperature, at discharge operation, because I'm going to use a purpose built LiPo charger. So, can I just use the discharge Mosfet to reduce cost? If yes, what do I need to do with the CHG pin at the schematic?
- At the datasheet I have seen that the over voltage is from 3 V to 4.5 V, what does this mean? Do I need to buy a specific IC, that comes with a specific over voltage level? Maybe I have not seen this information, if so sorry.
Thanks any help.