This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61029 Current Limit

Other Parts Discussed in Thread: TPS61029

Hi

We measured over current condition at the TPS61029.

Result is moved two operation current limit protection. 

Situation①

When increase to 1.3A, Vout is decrease to around the 1V. 

But the current is continue to flow around the 1.3A.

TPS61029 heat up(90℃) after a while.

Situation②

It suddenly becomes overvoltage when repeating low load and heavy load

The same state continues even if the electronic load is removed.

Vin:4.6V

Vout:6.7V

Iout:1.2A

TPS61029 heat up(90℃) after a while.

 

・Question

Could you tell me the operation of the TPS61029 over current limit protection?

Best regards,

masa0301