Hi Team,
My customer, one leading Power automation customer, is using our LM5025 in a new products. LM5025 volume should be 100ku/y with more than 5 years life time. LM5025 already be used in several products and now in one special application, customer hope to realize below requirement:
1. Using fly-back topology with 15V input voltage and 28~30V out;
2. Isolation between primary side and secondary side is 4500VDC, up to 10000V transient isolation requirement;
3. Customer can't use feedback isolator between primary side(input) and secondary(output) side because the high isolation requirement, that means it's open loop system;
Customer use our LM5025 in such application, but the duty cycle is changed a lot and the also the oscillator frequency is changed too, thus cause the output voltage changing from about 24V to 40V(When load current change from 0A to about 0.1A), Customer can't accept this variation. So not sure do you have some solution for this? Customer hope to get a stable output voltage in this open loop application.
If LM5025 can't realize this, I see we have LM5026 which is current mode. In our LM5026, the maximum duty cycle seems can be fixed by the PWM comparator, the programmable maximum duty cycle clamp and the line voltage. So if we can let customer use LM5026 work at just the maximum duty cycle point, like 60%.So the question are:
1. If this be possible? If so how to realize this?
2. If not, why?
3. Will this maximum change a lot?
Best regards,
Sulyn Zhang