Hello!
I have a problem with the design equations on the datasheet.
Eq (17) y (18) are the same, when they're setting different parameters.
Eq (17): R(iset1) = (Kiset1 x Viset1) / (Rsns x Icharge)
This eq seems to be OK, because pin ISET1 on BQ24125 sets the Output Current (Fast charge).
Pin ISET2 (according to PIN FUNCTION Table) sets the output current in precharge mode, or termination mode.
However, Eq (18) is EXACTLY the sam that Eq (17)
Eq (18): Eq (17): R(iset1) = (Kiset1 x Viset1) / (Rsns x Icharge)
And finally Riset1 = Riset 2!! That means Icharge = Iprecharge!
Which one should i take?
(There're several mistakes in datasheet)
PD: I have to design a 250mA battery charger, anyone have the values of Riset1, Riset2, Cout, Lout and Rsns?
Thanks!