Hi,
My initial plan is: Use LTC4015 to control charging activity on 24V lead acid battery from solar panel(its Max Power Point Voltage is 36V, and Open Circuit Voltage 45V). Since LTC4015's max input voltage is 35V, TPS54360 is used to regulate it's input volatage to 32V between solar panel and LTC4015.
The concerning about this plan are:
1.LTC4015's Max Power Point Tracking is not used directly in this plan because solar panel voltage output is not able to directly contect to LTC4015 input, but via TPS54360 regulating to 32V as input.
2.TPS54360 is not be able to provide Max Power Point Current because TPS54360 is a PWM controller.
I appreciate your any input to the concerning.
Thank you,
Gansheng