I am using the bq20z655-R1 in a 2s2p cell configuration and am having a problem. When I create the .senc file after running the optimization routine and attempt to program another board, I get the R_DIS bit ON and the VOK bit OFF. The same issue crops up if I extract a .rom image and use the Multi-Tester to program the board. What allows the VOK bit to become enabled? I have tried both charging and discharging the pack for several minutes and do not see the bit come on. Is it necessary to apply an IT Enable (0021) command to the pack even after batch programming?