This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi!
I was wondering if the TLV61225 can be operated in shutdown mode with VIN 0V or VIN > 0V while VOUT is supplied from another source and > 0V. The datasheet mentions this:
During shutdown, the
converter stops switching and all internal control circuitry is turned off. In this case, the input voltage is connected
to the output through the back-gate diode of the rectifying MOSFET.
Does this mean, that current from the output to the input is blocked by the internal diode?
Thanks,
Peter