This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE threshold and delay setting - ref apendix A in sluua04c

1) Why there are 2 threshold settings in every table . ?

2) what does RSNS =0  or 1 signify ?

  • Which tables are you referring to?

    RSNS is a parameter used with the hardware based protection parameters - AOLD and ASCD, to extend the current fault thresholds for these parameters. The SCDDx2 parameter extends the current fault reaction times for these parameters.