This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

power adapter board

Other Parts Discussed in Thread: LM5161, TPS54331

Hello,

We are designing a power adapter board.

It has TIVA mcu, sensors and buck regulators. The input to this board is from a constant current source 52 to 100V range @ 1A max

The power to the board (mcu) is taken from the CC source. we used LM5161 in the design to convert the input 52v to 100V to 12V.

TPS54331 is used to convert 12V to 5V  and 3.3V to power the onboard devices and mcu.

Kindly let me know whether LM5161 can be used with constant current input. if not could you kindly suggest a part for the same.

Regards,

Sumathi