This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ29707 (MRK F5) alternates at 35.6Hz at +0.09V on V-

BQ29707 MRK F5 does not set DOUT LOW at 0.1V on V-, but oscilates at 35.6 Hz = NOK.
Thus current limit is above 2Amps at 0.05+0.02 Ohms, Rsense + RFET. FET is CSD85302L.
COUT is LOW at -0.1V on V- =OK.
Over/Under voltage 2.8 to 4.28V is OK.
Please investigate and return to me asap, thanks.