This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MOS Parameters of DCDC

Other Parts Discussed in Thread: TPS53355A, TPS548A20, TPS53515, TPS53513, TPS54618, TPS54418, TPS54218

Hello,

      customer request MOS parameters typical value as below in order to calculate power loss. Could we provide that to customer? thank you.   

MOS Parameter
Solution Table Current H-Trise(nS) H-Tfall(nS) H-Qg(nF) H-Vgs(V) L-Trise(nS) L-Tfall(nS) L-Qg(nF) L-Vgs(V) Note
P12VIN_TPS53355A(PIN-TO-PIN) 30A                 Integrate(6X5mm)
P12VIN_TPS53353A(PIN-TO-PIN) 20A                 Integrate(6X5mm)
P12VIN_TPS548A20(PIN-TO-PIN) 15A                 Integrate(4.5X3.5mm)
P12VIN_TPS53515(PIN-TO-PIN) 12A                 Integrate(4.5X3.5mm)
P12VIN_TPS53513(PIN-TO-PIN) 8A                 Integrate(4.5X3.5mm)
P5VIN_TPS54618(PIN-TO-PIN) 6A                 Integrate(3X3mm)
P5VIN_TPS54418(PIN-TO-PIN) 4A                 Integrate(3X3mm)
P5VIN_TPS54218(PIN-TO-PIN) 2A                 Integrate(3X3mm)
                     

BR

Patrick

  • You will need to make an individual post for each IC with the part number in the title of your post. That way the proper person will know to look at your post. I can tell you right now that the information is probably not available though.