This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24295 charger: force the input source

Other Parts Discussed in Thread: BQ24295

We used TI BQ24295 charger in the product and it used an AC adapter for battery charging.

 

1) The USB D+/D- pins of AC adapter are shorted and connected to GROUND.

 

2) After we tested, the BQ24295 detected this AC adapter as USB host (in REG08[7:6]).

2-1) And BQ24295 sets the Input Current Limit to SDP (500 mA).

 

3) Is it possible to force BQ24295 to recognize/detect the AC adapter as “Adapter port”?

 

3-1) If the answer is “NOT”, could we force the “Fast Charge Current Limit”,

“Input Voltage Limit”, and “Input Current Limit” to 5V/2A  

even if BQ24295 recognized the AC adapter as an USB Host?

 

3-1-1) Are there any side-effect if we force the 3 setting to BQ24295 in 3-1) ?

 

Thank you.